Why Wait? Start Weaving These Connector Terms and Definitions Into Everyday Conversations Today! |
|
Back-mounted: A connector design used in panel or box applications in which the mounting flange is located inside the equipment enclosure. Bayonet Coupling: An interconnect mating design which utilizes pins on the receptacle and ramps on the plug to provide quick-connect and -disconnect coupling. "Reverse" bayonet puts the pins on the plug and the ramps on the receptacle. Circular Connector: Any of a thousand flavors of mulitpin interconnects with cylindrical contact housings and circular contact interface geometries. Circular connectors are selected for their ease of engagement and disengagement, their ability to conveniently house different types of contacts, their wide range of allowable contact voltages and currents, their ease of environmental sealing and their rugged mechanical performance. Note: One disadvantage of the circular design is the loss of panel space when used in arrays. In military and other high-reliability applications, the MIL-DTL-5015 and the MIL-C-38999 are the most commonly specified circular connector types. Closed Entry: A contact cavity design in which the ID of the socket insulator is smaller than the ID of the socket contact. Closed entry limits the size or position of the mating contact to a maximum predetermined dimension. Connector Body: The metal or plastic shell of a connector. Its main purpose is to house the contacts, maintain their position and shield them from dust, dirt, moisture, and electrical interference. Coaxial Contacts (and Cable): A contact equipped with inner and outer conductive elements separated by a center dielectric element. Coaxial contacts are used to terminate coaxial cable, and are typically employed in high bandwidth, high-frequency applications such as video and audio communications. The unique cable offers a closed, controlled impedance medium for the transmission of RF energy. It also provides robust electrical performance at high frequencies and naturally shields against Radio Frequency Interference (RFI). Contact: The conductive element in a connector. Contacts mate mechanically and electrically to transmit signals and/or power across a connector interface. Crimp style contacts are the most common type found in high-reliability cylindrical connectors. Male contacts are sometimes referred to as leads, posts or pins. Female contacts are universally known as sockets. Contact Arrangement: The gauge, number, spacing and arrangement of contacts in a connector. Contact arrangement selections are based on the current and voltage requirements of the application, and the space available for the connector package. Sometimes called the contact pattern. Contact Engaging and Separating Force: Tensile force required to engage or separate mating contacts. Measured in ounces, force increases with the number of contacts and with contact size. Contact (or Circuit) Identifier: Interconnect systems have multiple circuits and it is critical to be able to keep track of them from one end of the system to the other. Wiring schematics therefore identify and label each and every circuit with numbers, letters or special codes. On the connector, this process is maintained by marking (via silkscreening or other media) small numbers or letters next to each contact cavity, on both the front and rear of the connector. Contact Resistance: The measure of electrical resistance across a pair of fully mated contacts. Measured in ohms or millivolt drop at a specified current, contact resistance is affected by normal force (the static force on the contact interface), plating quality and the physical geometry of the contact. Contact Retainer: A locking clip or tang used to secure a crimp contact in place within the connector insert. Contact retention specifications define the force required to remove a properly seated contact for each class of connector. Contact Retention: The pressure or load a contact can withstand, in either direction, without being dislodged from the retaining clip which holds it in place within the connector body. Contact Size: An assigned number (such as #20 or #22) denoting the outside diameter of the engaging end of the pin contact. Like many other technical dimensions, the larger the number, the smaller the size. Contact Spacing: Also referred to as pitch, contact spacing is the distance, center-to-center, between adjacent contacts. Coupling Ring: An accessory feature of the connector plug which aids in mating and unmating plugs and receptacles and in preventing decoupling of the connector when in use. Typically a free-spinning threaded ring, coupling rings are also available in self-locking designs for high-vibration applications. Crimp: The physical compression (deformation) of a contact barrel around a conductor in order to make an electrical connection. Crimp Contact: A connector pin or socket, shipped loose with the connector body, and designed to be crimped onto the end of the wire conductor with a special tool. Sometimes referred to as "crimp and poke" contacts, the terminated contact is poked into the connector body either by hand, or in the case of small gauge wires, with the aid of a hand-held tool. Due to the ease of assembly and maintenance afforded by crimp contacts, they are preferred for all aerospace and other high reliability applications except those requiring a hermetic seal. Dielectric: A material having electrical insulating properties, such as the contact insulator in a connector or the jacketing on a wire. Electrical Connector: A separable device which provides mechanical and electrical contact between two elements of an electronic system without unacceptable signal distortion or power loss. Environmentally Sealed: The capability of connectors and backshells to prevent fluids, moisture, air or dust from degrading the performance of electrical contacts and conductors. "Environmental" interconnect components typically use gaskets, grommets, potting materials or interfacial and o-ring seals to prevent the penetration of foreign substances into the body of the part. Filter Contact or Filter Connector: Contact design which provides EMI suppression in addition to its normal function of transmitting electrical energy. Filtered connectors are typically specified for high-speed signal paths. Filtering is accomplished through the integration of capacitors into the contact to separate high-frequency noise from low-frequency signals. Firewall Connector: A class of high-reliability, feed-through connectors designed to prevent fire or sparks from penetrating through a sealed bulkhead. Firewall connectors must continue to function for a specific period of time when exposed to fire, and are typically specified in military applications such as fighter jets and Navy ships. Flange: The integral mounting plate on some bulkhead and feed-through connectors used to attach the connector to the chassis or panel. The connector flange is typically square, and is mounted to the panel with threaded screws. Front Mounted: A connector design used in panel or box applications in which the mounting flange is located on the inside or outside of the equipment enclosure. Front Release: "Crimp and poke" style contacts may be removed from the connector for maintenance using a special hand-held tool. The proper insertion and removal tool must be used at all times. In front release designs, the tool is inserted into the mating face of the connector to disengage the contact from its retaining clip. The disengaged contact is then removed from the back (cable-side) of the connector by lightly pulling on the attached wire. Grommet: An elastomeric seal used on the back side of a connector to seal out fluids, moisture, air and dust. Grounding (or EMI) Fingers: A set of spring fingers in certain connectors, used to facilitate shell to shell grounding and enhance EMI performance. The grounding fingers engage before contact mating and remain engaged until after contact separation. Guide Pins: Metal post(s) with a rounded or pointed tip which projects beyond the contact interface, used to assist in the correct alignment and mating of connector shells and contacts. The post mates with a corresponding cavity on the mating connector before contacts are allowed to engage. Guide pins are typically used in rack and panel packaging and in other "blind-mate" applications. Guide pins can also be used to insure correct polarization. Hermetic Connector: A class of high-reliability connectors equipped with a pressure seal for use in maintaining pressurized application environments. The hermetic element of the connector is typically fabricated from vitreous glass. Insert: A molded piece of dielectric material that fits inside the connector shell and supports the connector contacts. Inserts must be tooled for each size of shell, and each contact arrangement. In addition to holding the contacts in place, inserts made from resilient materials also contribute to the environmental properties of the connector. Insulation Displacement: A form of termination in which an insulated wire is pressed into a terminal slot smaller than the conductor diameter, displacing the jacket insulation to make electrical contact. Interfacial Seal: An elastomeric seal--generally found in the pin contact side of a mated pair--designed to provide overall sealing of the mated connectors and their individual contacts. "Cork and bottle" style interfacial seals feature a raised shoulder around each pin contact which compresses into the corresponding hole on the socket contact insulator. Key: A short pin or projection (sometimes referred to as a "dog" by crusty old machinists) which slides into a corresponding slot or keyway to guide the plug and receptacle together during mating. The principal function of the key is to insure polarization of the mating contacts. Levels of Interconnection: A classification system for connectors which defines connector types in terms of their role or function in the interconnect system. In other words, which points of the system do they connect? The levels of most use to us mortals include Level 4 (subassembly to subassembly), Level 5 (subassembly to I/O) and Level 6 (system to system). The lower levels (1, 2 and 3) all concern interconnection inside the microscopic world of circuits and boards. This approach to classifying connector types is particularly useful in interconnect system design, because it reminds the designer to attend to the environmental, electrical and mechanical requirements typically found at each level. Mating and Unmating Force: The force required to join and separate two halves of a connector. This is the sum of contact engaging forces plus any additional force necessary to overcome minor misalignment of connector halves and any dimensional variations in the connector shells. Normal Force: A measure of the spring pressure applied perpendicularly to contacts in mated connectors. The force of this spring pressure creates the gas-tight interface between contact surfaces which prevents corrosive contaminants from penetrating or forming between the contacts. High normal force reduces resistance across the contacts, but contributes to contact wear and may overstress the connector housing and even damage the spring properties of contact sockets. Maintaining a constant normal force is however an essential requirement for electrical integrity in the connector. Package Size: The length, width and height of the connector; or alternatively the dimensions of the entire interconnect system. Package size is an issue in many applications where system miniaturization, faster operating speeds, higher operating temperatures and other application requirements place new demands on the envelope of space the connector and its accessories may occupy. Plug: The half of a connector pair which is designed to attach to a wire or cable; as opposed to the receptacle half which is typically mounted to a bulkhead, panel or box. Even though we usually picture plugs as having male (pin) contacts, they can in fact house any type of contact--pins, sockets or even both. Thus it is the design and location of the connector which makes it a plug, not the gender of the contacts it contains. Polarize: Design features on mating connectors--such as keyways or shell geometries--that insure connectors can be mated in only one possible orientation. The shape of a D-Sub connector shell, for example, assures that the two halves of the connector can be mated in only one way. Potting: The permanent sealing of the cable end of a connector with a compound or material to exclude moisture or to provide a strain relief. Glenair typically uses epoxy compounds for this purpose because of their dimensional stability and high-temperature resistance. Rear Release: "Crimp and poke" style contacts (see Crimp Contacts above) may be removed from the connector for maintenance using a special hand-held tool. The proper insertion and removal tool must be used to install and remove wires from such crimp and poke connectors. In rear release designs, the tool is inserted into the rear (cable side) of the connector to disengage the contact from its retaining clip. The disengaged contact is then removed from the connector by lightly pulling on the attached wire. Receptacle: The other half of the connector pair, designed to be mounted--with jam nut fittings or other fastener hardware--to a bulkhead, panel, chassis or box. In-line receptacles are also available for cable-to-cable connections. As with the plug, it is the design and location of the receptacle in the interconnect system, not the gender of its contacts, which makes it a receptacle. Rectangular Connector: Any of the thousands of multipin interconnects with rectangular shell housings and rectangular insert interface geometries. Rectangular connectors are typically mounted in rack and panel configurations in which large arrays of fixed receptacle connectors are mated with plugs attached to a movable rack. The rack and panel configuration allows for efficient utilization of available space in applications where space is at a premium, such as in cockpit avionics. Other common uses for rectangular connectors are in the wire-to-board and board-to-board interconnection of PCB's and their I/O cabling. The D-Subminiature is the most ubiquitous rectangular connector in the world. Scoop-proof: Scoop-proof connectors feature a nice, long shell on the receptacle which prevents damage to the exposed contact pins during mating. No matter how hard that swabbie tries, it is impossible to cock the mating plug so as to damage the pins or electrically short the contacts. Service rating: Also called Current Rating, the maximum voltage or current load a connector is designed to carry during continuous, long-term use. Good engineering practice usually entails preliminary testing of connectors which will be operated with most or all contacts at the maximum rated load. Designers will often maximize contact and wire size in such situations. Solder Cup: A connector design that typically uses potting material to permanently affix the contacts inside the connector shell. Termination of contact to wire is then accomplished by soldering the wire into the cup-like barrel on the back of the contact. In the United Kingdom it is important to pronounce the "l" in solder. Brits also prefer to say "bucket" rather than "cup" when specifying solder contacts. Surface Mount: A termination method in which solder "tails" or leads on the connector are soldered directly to a printed circuit board. In high reliability commercial and military applications, surface mount receptacle connectors are typically limited to rectangular designs such as D-Subminiatures and Micro-D's. But some surface-mount applications do use a cylindrical connector mounted to the box with ribbon cable or flying leads soldered directly to the PCB. The reason here is to provide a low-resistance pathway to ground of the shielded cable. In severe EMI applications, it is less satisfactory to bring the shielded cable directly to the printed circuit board because of the difficulty in shielding out interference conducted along the cable. Termination: Termination is the physical act of attaching a wire conductor to a contact. Effective termination contributes to electrical performance and to the durability and reliability of the interconnect system. Common termination methods include crimp, insulation displacement, surface mount, and soldering. Termination can also refer to the mechanical attachment of EMI shielding to the connector backshell. Threaded Coupling: An interconnect mating design which utilizes a threaded nut on the plug, and a corresponding set of threads on the receptacle, to mate the pair of components. The coupling nut is usually equipped with flats or knurling for easy assembly. Different thread types, profiles and geometries provide different functionality. "Buttress" threads, for example, are often specified on plastic connectors due to their enhanced tensile strength. The MIL-C-38999 Series III connector incorporates a triple-start threaded coupling mechanism for greater vibration protection and faster mating and unmating. Wiping Effectiveness: Maintaining a clean, metallic path is essential if contacts are to perform with low and stable contact resistance. Happily, surface films and contaminants are removed from the surface of plated contacts each time mating occurs. This displacement of surface contaminants during mating is called contact wiping. Wiping effectiveness depends on the contact geometry, engagement length and normal force. Interestingly, oxide film does not form on gold plated contacts, so wiping pressure can be lighter to displace only the occasional surface contaminant. Wire Pull-Out Force: A connector specification which defines the force required to separate a wire from a contact. In properly terminated crimp contacts, the wire will generally break before it pulls away from the contact. |
| Glenair QwikConnect Navigator | ||
|
|
![]() |