Turn Off Your Radio
|
Electromagnetic interference can jam sensitive equipment, burn out electric circuits, and even prompt explosions. Which is why drivers are directed to turn off car radios when travelling through mining areas where electronically controlled blasting is under way. In aircraft, EMI can affect everything from fly-by-wire flight control systems to a cockpit fuel gauge, and in extreme cases put a plane into an uncommanded dive or shut down a critical avionic system. Whither EMI?
Naturally occurring radio noise originating from atmospheric disturbances (including lightning) and extraterrestrial sources (such as sunspots) can also degrade the performance of electronic equipment. Communications signals may also interfere with the operation of sensitive electronic equipment. To protect avionics systems from this class of interference, intentional radio frequency (RF) emitters like CB radios, remote-controlled toys, and walkie-talkies are banned outright on commercial airline flights. Most, but not all, airlines extend the ban to portable radios and television receivers. Personal Electronic Devices (PED) such as laptop computers, hand held scanners, and game players, while not intentional emitters, can produce signals in the 1 MHz range and can therefore affect the performance of avionic equipment. As navigation cabling and other critical wiring runs along the fuselage inside the aircraft skin, it's no wonder that passengers sitting just a few feet away are warned about the indiscriminate use of such devices. Since the thin sheet of dielectric material that forms the inside of the passenger compartment - typically fiberglass - offers no shielding whatsoever; and since commercial passenger jets contain up to 150 miles of electrical wiring, it is extremely important for passengers to heed regulations on the use of disruptive electronic equipment. Obviously, such internal sources of EMI are particularly dangerous to aircraft because they are so close to the systems they might affect. But external sources, such as radio and radar transmitters on the ground, or radar from a passing military plane, can be even more disruptive due to the high power and frequency of such equipment. As if the many external and internal sources of EMI were not enough of a concern, a major EMI co-conspirator in aircraft is the aluminum airframe itself, which in certain circumstances can act as a resonant cavity, or a phased array. Behaving much like a satellite dish, the airframe can compound the effects of both internal and external EMI by concentrating transient signals and broadcasting the interference into nearby equipment. Define Your Terms
In scientific circles, the terms "electromagnetic compatibility" and "electromagnetic interference" are used almost interchangeably: EMC simply describes efforts to control or eliminate the problems created by EMI. For commercial electronic and electrical equipment the Federal Communications Commission (FCC) has regulations defining allowable emission and susceptibility levels. Military equipment is regulated by MIL-STD-461 and MIL-STD-462 (refs 4-10 and 4-11). MIL-STD-461 defines allowable emission levels, both conducted and radiated, and allowable susceptibilities, both conducted and radiated.
A recent incident on a commercial passenger plane illustrates the power of even low frequency RFI to disrupt avionic systems. In January 1993, on a flight from Denver, Colorado, to Newark, NJ, an aircraft lost all directional gyros (electromechanical devices that indicate orientation) at cruise altitude. The captain instructed the flight attendant to go through the cabin and tell all passengers to turn off their electronic devices. She reported back that about 25 passengers with portable radios had been listening to a Denver Broncos playoff game and that one passenger was also using a lap top computer. Within two minutes of the Captain's request to turn the radios off, the gyros had swung back to their correct heading. Later in the flight, several Bronco fans covertly resumed their use of the portable radios, and again the directional gyros began to malfunction. The radios were then confiscated and no further problems were experienced on the flight.
When EMI and Avionics Meet
Glideslope Systems used during landings operate in the 328 to 335 MHz range. Distance-Measuring Equipment (DME), which gauges the space between the aircraft and ground-based transponders operate at just over 1 GHz. Also in the spectrum above 1 GHz are global positioning, collision avoidance, and cockpit weather radar systems. Personal Electronic Devices (PED) operate at frequencies from 10 to 15 KHz for AM radios and up to 400 MHz for laptop computers. When the higher harmonics of these signals are taken into account, the emitted frequencies cover almost the entire range of navigation and communication frequencies used on the aircraft - and PEDs are just a single class of EMI emitters. When the full spectrum of other radiated and conducted EMI emitters are taken into account, it becomes clear that the entire system of electronic equipment aboard commercial and military aircraft are at risk to EMI.
In many cases the cause is simply inadequate shielding, or shielding which has been damaged during servicing or has degraded due to corrosion, thus increasing the resistance of the electrical connection to ground. As effective shielding is dependent on good grounding, any additional resistance in the system - for example at a corroded backshell or a poorly installed shield termination crimp ring - can enable the wires to pick up interfering signals directly. Aircraft with navigation and communication antennas located outside the skin of the aircraft can also pick up EMI radiated through passenger windows and other unshielded openings in the plane. The pathway for RFI from a passenger PED would, in this example, be out the window, back into the plane via an unprotected or RFI sensitive antenna, and then directly into a navigation receiver, autopilot computer or other avionic device. EMI Management
In practical terms, EMI management is accomplished by plating the skins of cases and cable shields, building up the density (thickness) of shield material, or eliminating line-of-sight entry points through which electromagnetic waves can penetrate or escape.
Shields must also be effectively terminated to the connector backshell lest radiation enter the system at the backshell/connector/shield interface and defeat the purpose of the shield.
This transfer impedence test illustrates how high frequency shielding is improved by adding multiple layers of tinned coppper shielding to Glenair made metal core conduit. Shielding Solutions Cable shielding is manufactured in a wide range of designs and configurations. Each type of shielding has advantages which must be considered when selecting the best and most cost-effective option for a given application. Common cable shield materials include: Braided Shields: Braided shields provide exceptional structural integrity while maintaining good flexibility and flex life. Braided shields are effective at minimizing low frequency interference at audio and RF ranges. In use, the reduction of EMI is dependent upon the signal amplitude and frequency in relation to the many combinations of mesh count, wire diameter and the braid material. Generally, the higher the percentage of braid coverage, the more effective the shield against high-frequency emissions. Materials include tin-plated copper, nickel-plated copper and tin-plated iron/copper as well as hybrid materials such as metalized Kevlar (Aracon®).
Metal-Core Conduit: The "Cadillac" of EMI shielding, helically-wound metal conduit provides extremely high levels of EMI protection across all radiation fields and frequencies. Metal-Core Conduit is the material of choice for TEMPEST secure communications and other applications involving sensitive electronic equipment and intense levels of EMI. Available materials include brass, nickel/iron and stainless steel. The conduit is generally specified with overbraids of plated copper and rubber jacketing. The choice to use Metal-Core Conduit depends on the sensitivity of the equipment under consideration and other mechanical, thermal and environmental requirements. What About Fiber Optics?
|
| Glenair QwikConnect Navigator | ||
![]() |
![]() |
![]() |