QwikConnect Vol 10 Num 1 April 2005



Wearable Soldier Electronics

T he US military is undergoing a massive transformation driven by the need to develop new capabilities to conduct military operations in urban areas. A new doctrine, Military Operations in Urban Terrain (MOUT), identifies the key requirements and capabilities:
Increased Situational Awareness: “Where am I, where is the enemy and what are my orders?”
Increased Weapons Effectiveness: Maximize accuracy and minimize collateral damage.
Increased Individual Agility: Facilitate fast ingress and egress by unencumbering soldiers from heavy equipment.

 
Figure 1.

Figure 2.

Figure 3.

Figure 4.

Figure 5.

Figure 7.

Figure 6.

Figure 8.

Figure 9.

Figure 10.

Figure 11.

Figure 12.

Figure 13.

Figure 14.

Figure 15.

Figure 16.

Figure 17.

Figure 18.

Figure 19.

Figure 20.

Figure 21.

Figure 22.

Figure 23.

Example WSS Components

cutaway_plug

cutaway_receptacle


Advanced Wearable Soldier Systems (WSS) achieve an important, additional tactical requirement by enhancing the soldier's ability to share information with his squad and with command centers. The MOUT doctrine has expedited development of a new generation of “wearable” soldier electronics for reconnaisance, communication, fire-control and other critical operations. Simply put, these new technologies are designed to make today's soldier (and tomorrow's) more effective than ever before. Combined into complete operational systems (see figure 3), WSS depend on ruggedized and miniaturized electrical connectors capable of surviving the battlefield environment. In many respects, the various sub-systems are only as reliable as the ruggedized interconnects used for distributing power, data and audio-video signals between systems. Ruggedized connectors also facilitate fast replacement and repair of damaged systems—a critical capability in harsh, battlefield applications. This issue of QwikConnect presents a complete overview of WSS and the performance requirements of the battlefield. The report details Glenair's early involvement with wearable soldier electronics and the development of our Series 80 "Mighty Mouse" connector—a smaller, lighter alternative to D38999 and other Mil Spec connectors. Glenair's Series 80 has already been selected as a key component in Land Warrior and numerous other WSS platforms. Read on to discover why this miniaturized, poke and crimp connector has become the connector of choice for wearable soldier systems.

The History of Future Soldier Systems
An early version of an integrated soldier system appeared in 1989. The US Army Communications Electronics Command (CECOM) developed a prototype of a wearable computer integrated with a helmet-mounted display (HMD) and communications equipment. This system led to the development of the Land Warrior (LW) program "to improve the lethality, mobility, survivability, command and control, and sustainability of infantry soldiers." The first Land Warrior systems in the early 1990's were bulky, heavy and consumed too much power. These systems used microminiature connectors (.050 inch contact spacing) in the backpack electronics packages and nanominiature connectors (.025 inch contact spacing) in the helmet subsystem. These interconnects were costly and extremely fragile. Land Warrior underwent design improvements for next ten years, and will enter full production in 2005.

Glenair's Initial Role
Glenair manufactures a wide range of interconnect products for tactical battlefield use. These products include man-portable weapons cables, tactical fiber optic cable systems, conduit systems for wire protection on armored vehicles, environmental cables for field training equipment, as well as various ruggedized connectors and connector strain reliefs for shelters, missile and weapons systems. In 1999, Glenair was asked to develop light weight, ruggedized boxes to house batteries and the computer for JEDI, the Joint Expeditionary Digital Information System (Figure 1). The heart of the JEDI system is a ruggedized handheld compute. Other components include a GPS unit, laser rangefinder binoculars and a satphone used for target identification and transmition of the target type and coordinates to a remote joint command center. Circular receptacle connectors, with component parts and packaging modeled after the Micro-D interconnect, were used on the combination battery/junction box. Glenair also furnished the mating plug cordsets. US Army field trials exposed numerous weaknesses in the micro-interconnect design including inadequate environmental sealing and poor cable strain-relief (Figure 2).

Glenair proposed a new connector, with improved enviornmental performance and better accomodation for strain-reliefs and other backshell accessories. The new connector (which Glenair had first developed for aerospace instrumentation in 1997) proved to be ideally suited for ruggedized, Land Warrior applications. The Glenair Series 80 connector, also known as the "Mighty Mouse," offered virtually the same package density as the microminiature connector, but added environmental sealing, larger wire sizes, crimp-and-poke contacts, and other features found on traditional Mil Spec circular connectors. A key feature of this connector was compatibility with shielded cable and direct overmolding onto the connector (Figure 4). The original JEDI system evolved into a ruggedized personal digital assistant (R-PDA) computer (Figure 5). This computer is currently deployed in combat. Glenair recognized the potential for this connector in a variety of other battlefield applications, and by 2000, had begun to develop a broad family of these ruggedized, reduced size connectors for dismounted soldier applications. Environmental Performance Requirements Dismounted soldier equipment must be able to function properly when exposed to the harsh conditions of the battlefield, whether in the Arctic, the desert, or in a tropical jungle. Table I summarizes the typical performance requirements encountered in tactical deployment.

Table I: Soldier System Environmental Performance Requirements
RequirementMIL-STD-810F MethodDescription
Rain506.4Procedure I simulates rainfall at a rate of up to 1.7mm/min (4 in/hr.) with a wind velocity of 18 m/s (40 mph). Procedure II, the "firehose test", is also used. Equipment shall continue to function properly.
Sand and Dust510.4Procedure I evaluates the effects of blowing dust. Procedure II evaluates the effects of blowing sand. These tests are conducted on mated connectors.
Thermal Shock503.4Procedure 1 is normally used. This procedure cycles the device under test from cold to hot for a specified number of cycles. Battlefield equipment typically is cycled from -300 C. to +550 C.
Solar Radiation505.4Systems must not suff er excessive deterioration due to exposure to sunlight. No standard exists for simulating exposure to sunlight. Deterioration of materials is caused by a combination of environmental factors such as heat and humidity. Careful selection of materials known to be resistant to environmental deterioration is the usual way to meet solar radiation requirements.
Icing/Freezing Rain521.2Systems must function properly when exposed to snow or freezing rain. Specific interconnect test procedures have not been defined.
High Temperature501.4Systems must withstand continuous exposure to elevated temperatures. Battlefield requirements typically define high temperature to be +600 C. or less.
Low Temperature502.4Systems must withstand continuous exposure to low temperatures. Battlefield requirements typically define low temperature to be -320 C. Cables must resist cracking, and epoxies must withstand sealing degradation.
Fungus Growth508.5Equipment shall not support fungus growth or be damaged by exposure to adjacent fungus growth. This requirement is usually satisfied by careful selection of materials known to be resistant to fungus.
Salt Fog509.4Soldier equipment must resist corrosion from exposure to a salt fog atmosphere. Aluminum connector components are typically electroplated with corrosion-resistant coatings rated at 500 hours salt spray.
Water Immersion512.4All battlefield equipment must meet 1 meter immersion for two hours.
Explosive Atmosphere511.4Soldier systems must operate safely in the vicinity of fuel vapors without causing ignition. Contamination By Fluids 504 Soldier systems must withstand exposure to a variety of chemicals such as solvents, oils and decontamination fluids.
Shock516.5Systems shall withstand landing impact by a parachutist. Systems shall withstand operational shock of 40 g's and gunfire shock.
DurabilityN/ASoldier systems typically define an 18 year life cycle and a minimum of 2000 cycles of mating and unmating.
Breakaway CapabilityN/ASoldier systems require breakaway connections to meet specific release forces. Land Warrior systems require 15 pounds for the helmet and 20 pounds for the weapon.


Electrical Performance Requirements
Early Land Warrior wiring systems were much more complicated than today's version. For example, the original umbilical breakaway cable from the vest to the helmet had thirty coaxial lines requiring sixty contacts. Today's systems utilize commercial serial data protocols such as USB 2.0 and IEEE 1394. These protocols have greatly simplified interconnect wiring. One or two shielded twisted pairs, plus a power line and ground, are sufficient. Today's voltages typically do not exceed 50 volts DC, and current loads are usually under two amps, with battery power lines drawing up to five amps. Early soldier systems had coaxial cable extending from the torso-mounted GPS to a helmet-mounted antenna. Now, GPS units have integral antennas and the helmet umbilical connections no longer require a coaxial connection. Shielding is a primary concern. The US General Accounting Office identified electromagnetic emissions from cables and connectors as one of several major problems on the first Land Warrior systems. The US Army has established a requirement that soldier systems must meet MILSTD-461 radiated and conducted emissions from 2 MHz to 18 GHz. Conventional cable shielding techniques are usually sufficient to meet EMI requirements (Figure 6). Glenair Series 80 connectors have been shown to meet the EMI shielding requirements of tactical computer and communications equipment (Figure 7).

Connectors for Dismounted Soldier Equipment
A variety of connectors have been used for manportable tactical equipment. Connector types include: M24308 Type D-Subminiature Connectors: The popularity of the D-Sub connector and the low cost led to its use on handheld equipment. The installed cost increases once the connectors are fitted with the necessary shielding accessories. The D-Sub is difficult to seal properly. The drawn steel shells are not strong enough to withstand abuse. Thumbscrews are necessary to mate the connectors. (Figure 8) MIL-C-55116 and ā€œUā€ Type Audio Connectors: This field-proven family of connectors has typically been used on tactical radios including SINCGARS. The quick-coupling feature and spring-loaded contacts are the two primary advantages of these connectors. However, newer handheld digital tactical radios cannot use this connector because of the size. EMI shielding is also a problem. Breakaway versions are not available (Figure 9). MS Circular Connectors: M26482, D38999 and MIL-DTL-5015 connectors are widely used on tactical equipment. These MS connectors are not suitable for use on wearable equipment because of their size (Figure 10). M83513 Type Micro Connectors have been used on a number of wearable soldier systems including the MILES training gear. The connector size is ideal, but the contact system is prone to damage from sand and dust. The maximum wire size is #24. Attaching shields adds labor and cost. Glenair is reluctant to recommend this connector for battlefield use because of the potential for contact damage caused by debris entrapment. However, when small size is more important than other considerations, the microminiature contact can be successfully incorporated into ruggedized connector packages (Figure 11). Commercial Quick-Disconnect Circular Connectors: Several European manufacturers offer a variety of miniature connectors used on medical and test equipment. Their size, weight and quick release mechanism are appropriate for wearable soldier equipment. However, assembly is time-consuming, and these connectors are not as rugged as required for most battlefield applications (See figure 12).

Product Overview: The Series 80 "Mighty Mouse" Connector System
The Glenair Mighty Mouse connector is a miniaturized version of a Mil Spec type circular connector. It is approximately half the size and weight of the Mil-DTL-38999 Series III. The Mighty Mouse connector family is designed around a size 23 contact system derived from MIL-C-39029. The socket contact is a split-tine type with a stainless steel hood to prevent contact damage. Contacts are crimped using standard M22520 tools and are snapped into the connector housings. Printed circuit board receptacles are standard. Solder cup versions are also available. The size 23 contact accepts size 22 AWG wire through 30 gage wire. Glenair currently offers 10 contact layouts ranging from three contacts to 85 contacts. The insert assemblies feature beryllium copper retention clips captivated between rigid dielectric insulators. Flourosilicone face seals and rear grommets are bonded to the insulators. The Series 80 family has grown to include five connector styles to suit differing packaging, coupling, ergonomic and performance requirements. These five styles are shown in Figures 13 to 17. All Mighty Mouse connectors are available with a variety of plating finishes, and all types are available with an integral shield attachment and overmolding feature. This feature allows direct attachment of the cable without the need for bulky added-cost backshells (figure 18). The cutaway view on pages 12 and 13 shows the internal construction of the Series 80 connector.

MIL-STD-810F
Whatever connector type is selected, the equipment must meet the requirements of MIL-STD-810F. This specification covers a broad range of electrical, mechanical and environmental tests for system-level, subsystems and components. This comprehensive specification does not specifically address interconnect performance requirements, but serves as a basis for tailoring interconnect tests as necessary to validate their suitability for soldier systems.

New Series 80 Product Developments
Glenair continues to expand the Series 80 product line with new insert arrangements. These new layouts include 13 and 26 pin connectors, along with coaxial and power arrangements (Figure 19). Also new for 2005 is the Series 805 triple-start connector. Featuring 1/2 turn to full mate, the Series 805 also features a detent (clicker) mechanism in the plug, along with an EMI spring on the plug barrel (Figure 20). Glenair has also developed a new hybrid "MicroMouse" connector which incorporates Glenair's TwistPin microminiature contact into Series 80 connectors. Glenair currently offers a 55 pin arrangement in a shell size 9 connector (Figure 21). Although the TwistPin can be susceptible to damage from debris contamination, it offers a solution when connector size takes precedence over other considerations. This 55 pin connector is deployed on a tactical imaging system. Right angle header receptacles for printed circuit boards are also available. Note the unique rectangular mounting (Figure 22). Glenair has developed standard overmolds and cable to support rapid prototyping and pre-production of overmolded cordsets. A typical overmold tool is shown in Figure 23. The Series 80 product line expansion has led to a major ongoing program to increase component capacity and assembly capability. Most importantly, Glenair is adding hundreds of Series 80 connectors to Same Day stock.

Table II: Wearable Soldier Systems: Interconnect Problems and Series 80 Solutions

The table below summarizes the interconnect problems encountered with wearable soldier systems and explains how the Series 80 Connector addresses each issue:
Interconnect ProblemSeries 80 Solution
Connectors must meet EMI requirements Integral shield attachment feature or thread-on adapters.Low shell-to-shell resistance. Metal-to-metal shell bottoming of plug to receptacle.
Mated connectors must be watertight when tightened by handReceptacles feature a peripheral seal capable of 1 meter immersion.
Unmated receptacles must be sealed to withstand immersionPrinted circuit board receptacles are epoxy-sealed to meet 1 X 10-4 cc/ second leak rate. Wired receptacles must be specially potted. O-rings for sealing jam nut flanges.
Connectors must be matte black, and the finish must be conductiveBlack zinc-nickel plating over electroless nickel. Sandblast on exposed surfaces to reduce reflection.
Connectors must withstand up to 400 g's of shock from weapon firing without looseningPlugs fitted with extra-stiff wave springs to prevent decoupling.
Connectors should stay fully mated.Wave spring in coupling nut to prevent unintentional loosening.
Connector protective covers should not be metallic (noise) and should be black, non-reflectiveRubber covers with black oxide finish on attachment rings.
Connectors must withstand exposure to chemicals and salt fogAerospace grade materials and 500 hour salt spray finishes.
Connectors must support up to 1 gigabit per second data ratesThe short contact system minimizes bit error rates and is capable handling of gigabit ethernet signals.
Mated connectors must withstand 100 pound pull test on the cableThe Series 801 double-start thread has met this requirement. Proper cable selection and termination are important.
Breakaway connectors required for helmet, weapon and batteryGlenair Series 804 QDC version with adjustable release forces for specific needs.
Connectors must withstand temperature extremesField-proven military grade design and construction, high-temperature materials.
Connectors must be durableTested to 2000 cycles with no mechanical or electrical degradation.
Connectors must be easy to terminateContact system is identical to standard MS connectors.
Connectors must offer a grounding pin that mates first (LW requirement)Special connectors with extended pins were developed to meet this requirement (consult factory).
Connectors must be scoop-proofAlthough some Series 80 connectors are not scoop-proof, the smaller sizes used in soldier systems are scoop-proof.
Connectors must be readily available6-8 weeks lead time, many items in stock for immediate delivery.



Future Possibilities
Although today's wearable soldier systems are only just reaching the battlefield, the US military is already planning for future implementations to be deployed in ten or fifteen years. A primary area of interest is the concept of integrating electronics into the soldier's clothing and vest. The electronic hardware disappears into the fabric. Military futurists envision a triple-layered combat uniform. The outer layer provides ballistic protection, the middle layer conducts power and signals to various devices, and the inner layer monitors body temperature and soldier vital signs. This vision of an electronic uniform will likely be tempered by the realities and practicalities of manufacturing and function, as well as the need to plan for continuing electronics improvements. Electronics packages must be easily removed for repair or upgrade. A more likely scenario consists of small, lightweight electronics modules that are designed to fit into body-fitting protective pouches. A future generation of wearable soldier systems will require a new generation of interconnects. Connectors and cabling inside the vest will be either flat or ultra-miniaturized round, and will achieve environmental and electrical performance comparable to present systems. Glenair is already developing new connector designs–including nanominiature solutions–to meet next generation systems needs. Future helmet and weapon systems will continue to require rugged, reliable breakaway connectors. And in this area, Glenair is exploring ways to improve resistance to debris entrapment.

Summary
Wearable soldier systems present a unique set of challenges for interconnect systems. Glenair is proud of its leadership role in the development of interconnect solutions for wearable soldier systems. The Series 80 "Mighty Mouse" continues to evolve to meet today's and tomorrow's needs for miniaturized tactical and aerospace connectors.

  Glenair QwikConnect Navigator  
Previous
Next

Home Same-Day RFQ Product Sales and Services QuikConnect: What's New at Glenair Feedback