Series 80 "Mighty Mouse" Contacts and Tools

Series 80 Mighty Mouse Contacts and Tools

A Complete Assortment of Signal, Power and Coaxial Contacts and Termination Tools

This section of the catalog contains ordering information for contacts. Series 80 Mighty Mouse connectors are supplied with a full complement of crimp contacts. Contacts are terminated to wire using special tools and are snapped into place by hand or with a hand-held insertion tool. Damaged or miswired contacts may be removed from the connector using special extraction tools.

Although the connectors are supplied with a full complement of contacts, extra contacts are commonly purchased as spares or to use for quality assurance purposes such as crimp tensile tests.

Coaxial contacts must be ordered separately. If your application requires coaxial contacts, select contact types "A" or "B" (pin or socket) in the connector part number. The connector will be supplied without contacts. Select the appropriate coaxial or pneumatic contact from this catalog.

Aerospace Standard AS39029

Mighty Mouse contacts conform to the requirements of Aerospace Standard AS39029. This SAE specification defines the design, dimensions and performance of contacts used in aerospace grade electrical connectors. The "general specification" covers a variety of contacts including thermocouple, hermetic, coaxial and triaxial types.

"Slash Sheets"

Slash Sheets contain dimensions and other information for specific types of contacts. Each contact is assigned a Basic Identification Number (BIN), a nonsignificant three digit code corresponding to the color code on the contacts.

A Qualified Products List (QPL)

A Qualified Products List identifies those manufacturers whose products have been verified to meet all requirements.

Series 80 Size #23 and Size #20HD Contacts

Series 80 Size #23 and size #20HD contacts conform to AS39029 requirements, but are not covered by a slash sheet. Size #20, #16 and size #12 contacts are standard AS39029 contacts.

About Crimp Tools

Series 80 signal, power and coaxial contacts are crimped to wire using mil spec crimpers. Military Specification MIL-DTL-22520 provides the aerospace/defense industry with a common set of rugged, reliable hand crimp tools. This specification controls the voltage drop and tensile strength of crimp terminations.

Before ordering, check to see if you might already have these tools!

We have listed the military part number and the Daniels part number. Daniels Manufacturing Corporation is the leading manufacturer of these tools. However, size #23 and #20HD contacts require special positioners unique to the Mighty Mouse product line.

Related Catalog

Product Selection Guide
853-015

853-015

Size #12 Diferential Twinax Socket Contact for use with Mighty Mouse and Series 79 Micro-Crimp
853-016

853-016

Size #12 Diferential Twinax Pin Contact for use with Mighty Mouse and Series 79 Micro-Crimp
Size #23 Crimp Contacts

Size #23 Crimp Contacts and Instructions

#20, #16, #12 Contacts

#20, #16, #12 Contacts

Coaxial Contacts

Coaxial Contacts

Matched Impedance Coaxial Contacts

Matched Impedance Coaxial Contacts

Pneumatic Contacts

Pneumatic Contacts

Grommet Sealing Plugs

Grommet Sealing Plugs

Adapters, #20HD Contacts

Adapters, #20HD Contacts

Adapter for Crimping #20 AWG Wire to Size #23 Contacts
Crimp Tools and Positioners

Crimp Tools and Positioners

including for Coaxial Contacts
Contact Insertion and Removal Tools and Contact Retention Tester 809-107

Contact Insertion and Removal Tools and Contact Retention Tester 809-107

BAND-IT Shield Termination Tool Bands and Instructions

BAND-IT Shield Termination Tool

Bands and Instructions
Jam Nut Tightening Tools Connector Holding Fixtures

Jam Nut Tightening Tools

Spanner Tool for Tightening Series 80 Jam Nuts
Jam Nut Tightening Tools Connector Holding Fixtures

Connector Holding Fixtures

Connector Holding Tool for Tightening Backshells and Accessories
Glenair, Inc. 1211 Air Way, Glendale, CA 91201-2497 | Tel: 818-247-6000 | Fax: 818-500-9912 | Email: sales@glenair.com
Copyright © 2001-2012 Glenair, Inc. All Rights Reserved